LTE FDD
Configures the outputs of waveform. The button is located at the upper bar, invoke Output Configuration dialog.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:OUTPut:CONFig ANT1|ANT2|ANT4 [:SOURce]:RADio:LTEFdd:WAVeform:OUTPut:CONFig? |
|
SCPI Example |
:RAD:LTEF:WAV:OUTP:CONF ANT2 :RAD:LTEF:WAV:OUTP:CONF? |
|
Notes |
For query, also refer to Output Configuration in Waveform Basic. |
|
Runtime Apply |
No |
|
State Saved |
Yes |
|
Preset |
ANT1 |
|
Range |
1 Antenna | 2 Antennas | 4 Antennas 1 Antenna | 2 Antennas for Real-Time Uplink capability |
|
Initial S/W Revision |
A.14.00 |